This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Low ripple Boost converter

Other Parts Discussed in Thread: LM7332, TPS61023, TPS61022

Dear *,

we are looking for a boost converter IC with low output voltage ripple , lower than 10mV RMS.

The peak current load is 1A/50ns ( OPAMP LM7332 is supplied with the boost output voltage , and the output of the OPAMP is connected to the load  ). ( This is used for BIAS voltage)

Vin : 3.2V to 3.4V

Vout : 3.6V

would you recommend one of the two following devices:

TPS61023
TPS61022

Best Regards,

David.