Hi,
Customer is using shipping mode with the following steps:
Step1.With VBUS power supply and with BATFET connection
Step2. Write “1” from the host MCU to REG07 [5](Instruct the Shipping Mode transition in BATFET_DIS)
Step3. BATFET_DIS disconnects BATFET to generate SYS voltage from VBUS feed only
Step4. SYS voltage is lost due to VBUS disconnection and power supply to MCU etc. is completely stopped (= product transportation mode)
A problem occurs while using BQ25601 in the above step.
Could you give me some advice on the following questions?
1.After using "BATFET_DIS", if BQ25601 fails to turn off BATFET, can I check it in the internal register information?
Or can the above status be grasped by the INT signal?
2. Is it possible that BATFET_DIS does not disconnect the BATFET due to the effect of multiple processing inside the charging IC?
Is there any case where Sipping mode was not enabled, not limited to BQ25601?
Best regard,
Yusuke