This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25703A: Cutting current while input source is present

Part Number: BQ25703A

Hi,
I am using 18650 single cell battery and 12V input in my system. After the system works in the field for a while (1-2 days or 7-8 hours), it stops drawing current from the 12v input adapter. And it continues to run on battery and turns off when the battery runs out. When I power off my adapter and turn it back on, both the system works and the battery charges normally. And it keeps repeating like this.


Anyone experiencing this situation? What could be the reason for this or how should I improve FW or HW to avoid this situation?

Thanks

  • Hi Mahmut,

    Thanks for reaching out.

    Did you read any fault conditions in the registers when this occurred?

    Recommend to check the register list for any fault conditions.

    Peng

    *If my answer solves your question, please press "This Resolved My Issue" on the thread.  

  • Hi Mahmut,

    It has been a a week since this question was asked. There were not any replies from you so I assumed this problem is resolved.

    If you have more questions, feel free to start a new thread and reach back to us on the TI E2E forum.

    Thanks and I hope this helps,

    Peng

    *If my answer solves your question, please press "This Resolved My Issue" on the thread.