This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLC6983: TLC6983

Part Number: TLC6983


Hi,
Project requirements:
1. LED matrix driving (NO RGB,all same color LED)
2. VCC-3.3V
3. SPI Interface in daisy chain
4. LED current- 40mA
5. LED Open/short detection
6. PWM dimming
7. Auto scanning
I checked TLC6983 IC datasheet for our application. It fits all our requirements except the current sourcing capacity. (20mA)
Is there any way we can use external transistors to drive LEDs up 40mA each current? If yes then how the Dimming will work.

8. The datasheet of TLC6983 Says connecting two ICs in daisy chain.

9. Can I connect 10 of TLC6983 In daisy chain, does it support this?

10. When I connect 10 in daisy chain, does it support 10MHz clock speed?

11. If I connect transistors amplifier to support 40mA, I can not use brightness control function. So is PWM control is the way to control the LED brightness?

Thanks

Parvin