Other Parts Discussed in Thread: TSM103, TPS2413
Hi,
1. Can the voltage of UCC39002 PIN8 is divided as the reference voltage for TSM103 Pin5, as shown in the figure below?
Or it can be used by TSM103 without a voltage divider resistor?


2. Is OK for TPS2413 to drive two MOS? Or do I need two of TPS2413 to connect MOS separately?

Waiting for your feedback, thanks, and regards.