Dear sir ,
In the document tida01407 what is the role of diode D4 and D5 ?
Regards
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dear sir ,
In the document tida01407 what is the role of diode D4 and D5 ?
Regards
Hello,
Those diode provide a path for the difference in primary transformer current and the shim inductor when the design comes out of freewheeling.
If you do not have these diodes this extra current will cause excessive voltage across the primary of the transformer; as well as, your secondary FETs.
These clamping diodes are necessary for the phase shifted full bridge controller to operate correctly.
Regards,
Thank you for your reply sir .
While selecting these diodes as I can see its voltage rating must be similar to that of primary side MOSFETS. what about the current ratings of these diodes . I cant be able get a clear picture of average current rating of these diodes ??
Hello,
To select these diodes I would select them so they can handle the primary peak current of the Hbridge. You could set the RMS current to be similar to the primary H Bridge FETs. Most design
I gave this some thought. The current going through the diode when the transformer is first energized should be the difference in reflected output current ripple.
Iclamp_diode = (ILout peak)*Ns/Np - ((1-D)/fs)*Vout/Lout
The energy that needs to dissipated through these diodes is the shim inductance (Ls) and leakage inductance (Llk)
W = (1/2)*(Llk+Ls)*Iclamp_diode^2
You could estimate that the power dissipated by this diode is energy times switching frequency (fsw) of the primary
Pclamp_diode = W*fsw
Do be safe I would add a factor of 1.5.
You could also get a better estimate realizing the shim inductor is clamped to 1V.
dt = (Llk+Ls)*Iclamp_diode/1V
I would estimate that the current is triangular in shape so you estimate the RMS current based on a triangle.
Idiode_clamp_rms = Idiode_clamp* (dt/(3*fsw))^0.5
Regards,