Other Parts Discussed in Thread: BQ78350-R1, EV2400, BQSTUDIO, , BQ78350, BQ76930
I have a BQ78350-R1 evaluation board that I have configured for 7 series cells. I had 7 cells running a discharge log over night. When I got in, the cells had discharged to below 1V and the BQ software had locked. I forced it to quit and removed the dead cells, replacing them with a fresh pack of cells, but now the BQ software will not acknowledge that there is a powered board connected. The board boots as expected (the discharge FET turns on when TC1 is pulled low by pressing the boot button, and i'm getting 2.5V at Vreg out.( The charge FET won't turn on, however-- not sure if that's relevant)
I've also tried using a power supply instead of cells. Same result: No acknowledge from the device.
I've tried the EV2400 and eval board on a different computer, same result.
I've tried resetting the EV2400, same result.
I don't think the eval board is bad-- the voltages that should be present appear to be present. Is there a way to check to see if the EV2400 is dead? Am I missing something with the eval board?