Hello,
In order to achieve high start-up switching frequency, I set up UCC256404 with option 5.
The startup switching frequency is around 500kHz and I'm satisfied with it. However, the LLC converter cannot enter burst mode even under no load.
I suppose this is due to low BMT_H/BMT_L, but I'm not sure how to increase them. The formulas in datasheet 8.2.2.19 assume a Vssinit, which is 0 with option 5. Your excel spreadsheet calculator uses a protected table I have no access to. Can you let me know which direction I should try in terms of adjusting circuit parameters?
Below are my converter parameters and UCC256404 circuit parameters:
Vin = 385V, Vo = 22V, Lr = 42uH, Cr = 13.2nH, Lm = 400uH, Po = 250W
C_VCRup = 10pF, C_VCRlo = 1.8nF, C_LL/SS = 220nF, R_LL/SSup=180kOhm, R_LL/SSlow=100kOhm
Thanks you,