This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLVM13630: PTLVM13630 vs TLVM13630?

Part Number: TLVM13630


Team,

I assume that the both PTLVM13630 (Engineering samples) and (TLVM13630) RTM devices are based on the same silicon. Correct?

The main difference between the two would be that only RTM device is tested against the latest datasheet specification. Correct?

Are there other notable differences between the two?

Thanks in advance,

A.

  • Hello Anber, 

    Yes, these are the same devices. The "P" devices are pre-production (engineering samples). Once the device is RTM'd, the P is removed from the part number. There are no other differences between these devices.

    Regards, Jason