Part Number: BQ25798
In BQ25798, we are using backup mode. Load connected at PMID. Load consumes 5.1V & 1A. While switching from normal mode to backup mode, Load get restarted.
We are using 1S battery with 1.5MHz switching frequency.
We are using Single Input Source, Back Up Mode and No Ship FET.
How can I resolve this restart issue?
Image1: . Channel1-VBUS & Channel2-PMID (While go to Backup mode) (Main Goes to zero) 
Image3: Channel1-BAT & Channel2-PMID (With Mains)(In normal mode)
Image4: Channel1-BAT & Channel2-PMID (No Mains)(In backup mode)