Hello, I assembled two PCB's using baseline of the evaluation board and I am having following issue:
Charger does not provide more than 1600mA to the battery and above that value the inductor starts emitting sound like a buzzer and current register is unstable. My design is a copy of the evaluation board of this device. Please need help to understand what is causing this and hw to fix it. In fact I assembled 2 PCB's and both have same issue (both are set for using 3 cell 10.8V Li-ion battery). Attached is my schematic.
This happened in both PCB's but after a while one of them stopped working even having 12V at VIN or VBUS the device do nothing, charger OK LED does not turn on and I dont have voltages at VREGIN.
Also no I2C comms allowed.
Thank youCHARGER_MODULE_FOR_PWR_DIST_REVA.pdf