Hi TI Team,
Could we modify T1-T2 and T3-T5 temperature definition besides flexible charging voltage/ current settings (beyond the JEITA requirement)?
Thank you very much,
Mickey
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi TI Team,
Could we modify T1-T2 and T3-T5 temperature definition besides flexible charging voltage/ current settings (beyond the JEITA requirement)?
Thank you very much,
Mickey
Hi Mickey,
Some of our other chargers (such as the BQ2561x family) can adjust the JEITA_VT2 and JEITA_VT3 thresholds, but the BQ25883 cannot do this. With the BQ25883, you can shrink or expand the entire T1-T5 temperature window proportionally (for example, setting the charging window between 0-45 °C instead of 0-60 °C), but you cannot adjust the T2 and T3 thresholds independently.
Best regards,
Angelo
Hi Angelo,
Regarding the adjustment of (T1~T5) window, we definitely adjust RT1 & RT2 resistance respectively, e.g. using 9.31KΩ & 390KΩ to
proportionally shrink the window as 0-45 °C, in that case, does the TS pin of BQ25883 has max. limit of combination resistance (RT1 + RT2)?
Sincerely,
Hello Mickey,
Between 45-60degC should be fine, what temperature are you looking to set it at? There is maximum value, if you try to calculate the RTx values and get negative or over 1Mohm resistances then you have passed the maximum.
Sincerely,
Wyatt Keller
Hello Keller,
We'd like to charging our battery pack (with NTC thermistor 10K+/-1% at 25 °C) in 0-45 °C range and use 9.31KΩ (1%) & 390KΩ (1%) as RT1 & RT2 respectively,
Hope they still are good for the TS pin of BQ25883.
Sincerely,