Hello Team,
customer wants to use the DCDC converter for a short time (<300ms) with Vin lower than Vout due to voltage drop specification in his application.
As we do not have a 100% duty cycle mode in this converter - is it possible to describe what happens with output voltage during this voltage drop at Vin?
Specification is:
Vin typical is 14V..36V (load dump 58V)
Vout is 7V
Current max. 100mA
there is a voltage drop downto 6V for 300ms specified. What happens now with the output voltage? An output voltage down to 3.8V would be ok.
Many Thanks
Josef