This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS92692: Replacement for MAX20052

Part Number: TPS92692
Other Parts Discussed in Thread: TPS92520-Q1, LM3409, TPS92515

Hi Team,

I am looking for a replacement for MAX20052.

Vin = 5...24V
Vout ~ 5V
Iout ~ 300mA
Analog dimming needed
Small package size

Can you please recommend a device?

Thank you!

  • Hello Stefan,

    Thank you for reaching out. We have a couple of devices that could be a good match depending on the more detailed technical specs of the project, but the TPS92520-Q1 device is a dual-channel 1.6A synchronous buck that has analog dimming in an 8.1x11mm package. I have linked to the datasheet here. Please let me know if you have any other questions.

    Best Regards,

    Caroline

  • Thank you Caroline!

    MAX20052 has a package size of 3.1x3.1mm.

    Could you please also recommend something in that range?

    Thank you!

  • Hi Stefan,

    Our TPS92515 device and our LM3409 device both have package sizes that are 3x3mm. The TPS92515 is a monolithic, single-channel buck with analog dimming, but is not synchronous. The LM3409 device is a single-channel buck controller that is also not synchronous, but it can handle currents up to 5A.  

    I would like to point out that the TPS92520-Q1 is dual-channel so, although it is larger than the 3.1x3.1mm, when considering the fact that you would need 2 Maxim devices for each TPS92520-Q1, the size difference is significantly smaller.

    Best Regards,

    Caroline