Part Number: BQ79616-Q1
Hi,
looking at the following image and imaging that I want to balance two adjacent channels, it seems that if I try to do that, then the upper channel cannot turn on the external mosfet so the balancing phase cannot start in the upper channel. This is due to the current path that does not generate a voltage drop on the intermediate Rbias resistor so it does not turn on the upper mosfet. In other terms a whole "blue" current flows in the following path:

If I try to balance multiple adjacent channels the assumptions get more complicated.
- Are my assumption correct?
- Which is the best way to balance adjacent cells? I have to use them in an alternating mode?