On the TPS62088 datasheet, figure 23 shows the transient response of the IC. The response I am witnessing is a bit different. The conditions I am working with are a little different from those specified on the data sheet as well. Vin = 5V, Vout = 3.3V. I have attached some scope captures of the transient response I am seeing. Yellow is Vin, 5V. Green is Vout, 3.3V. Pink is Iload. My Vin looks more similar to your Vout. Just curious if something is abnormal here with these measurements. An electronic load was used to provide the transient response.
Thanks,
Ryan S.