Is it possible to output -15V with 15V input?
What is the wiring example at that time .
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Is it possible to output -15V with 15V input?
What is the wiring example at that time .
HI
yes, it can configure to inverting buck boost, but output capability will be less than 0.5A.
what means wiring example?
Thanks
Hi Aari:
you can refer below apps notes for inverting buck boost design with buck converter
Thanks
thanks reply.
Does this mention TPS54140?
Hi Arai:
it is a design guild how to configure a buck converter to inverting buck boost converter and what need to pay attention. even it doesn't mentioned about TPS54140, and it is a good design guild for TPS54140 configuration to 15V in and -15V out.
Thanks
thanks reply Daniel.
[ Minimum VIN for defined output typ 0.95V max 1.5V ] on TPS54140 datasheet
It has been described as.
Does this mean that it must be 0.95V lower than the input 15V?
For example, is the maximum output of 15V input 14.05V?
Based on that, I thought that I could not output -15V with 15V input.
I'm waiting for a reply.
Arai:
for 15Vin, -15Vo , duty is 50%, pls take close look at the apps I linked, so that you can know how the inverting buck boost works.

Thanks