Other Parts Discussed in Thread: USB2ANY, , BQ24650
Unfortunately my TI Charger GUI V1.4.3 now has some issues which prevents me from proper continue this test.
I got asked to update the Chrome Add-On which I did successfully. I am also able to connect (says Connected in green) and I could start setting it up.
But the data is not synchronized properly. No matter how I set "Auto Read" and "Write Mode".
I now got it charging but the GUI says it is not charging. Other data is also not updating the way it should. Strange.
For the second issue: It was connected to a 9V/ 10W Solar panel. It worked with no issue one full day but then the next day it did not start charging at all. While Vin was >8V (measured).
After disconnect/ reconnect the panel it started immediately. I guess that is not meant to be this way?
My IC is revision 7 if that matters.