Other Parts Discussed in Thread: BQSTUDIO
Hello,
I have been working on an external battery pack with BQ40z80. I was setting up the parameters in the data memory and the device went into shutdown mode.
I am not able to re-establish a connection with the pack using the BQStudio to reupdate the data memory or re-program the firmware.
Battery pack configuration 1P4S (1100mAh @ 13.6V) LiFePo4 chemistry.
I checked using an oscilloscope PBI and PACK pin.
Pack pin is working fine, PBI is getting set to around 9V.
DSG FET is not being enabled.
My first guess: Shutdown Voltage > Valid update Voltage (by mistake i set the Shutdown voltage to 8000mV)
In case the data memory parameters are casing the immediate shutdown is there a way to recover the normal operation of the device?