This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25606: Alternatives with an Integrated LDO

Part Number: BQ25606

Hello TI Community,

I'm using the BQ25606 Standalone 3.0-A Single Cell Battery Charger with a 270mAh battery and a micro-USB connector connected to the VBUS as charger input voltage (D+ and D- left unconnected).

 

The VSYS output is connected to the input pin of the IC charger for another pcb that runs on a 110mAh Li-Po battery. However I'm facing an issue at the moment: as VSYS output follows VBAT (minus the current drop on the  Rds if OTG function is used) I can't meet the VIN requirement for enabling the charger for the 110mAh battery as a VIN_min=4,5V is needed.

Considering that the battery is only 110mAh, at a rate of 0.5C, a 50mA current will be enough to charge the battery in a reasonable amount of time. I came across this IC with integrated LDO - BQ21062 which has a configurable load switch and power path. But it requires an host controller.

Is there something available that doesn't involve the use of an host? So I'm thinking about a standalone charger that has a Load Switch/LDO output capability.

Thank you,

Francesco