Part Number: LM5175
Other Parts Discussed in Thread: LM5176
Dear Ti Support!
We are working on a power supply with LM5175:
- input: 19-33V
- output: 24V @ 9 A
The output is working fine in buck and boost mode.
The only problem is that the LM5175 draws about 85mA current from 26V input voltage and it gets hot (about 60 C) with no load condition.
Do you have any idea what can cuase the big current consumption?
We tested on 2 borad, guess its not a soldering issue.
Thank you
Best Regards,
Gabor