Hello TI team
See attached image
Red is the input signal
Green is the output signal. Max load I connected was 4 Ohm. Component TPS4H160 has burned out. Why how I protect the component
Thanks
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello TI team
See attached image
Red is the input signal
Green is the output signal. Max load I connected was 4 Ohm. Component TPS4H160 has burned out. Why how I protect the component
Thanks
Hello Haim,
The device is designed to operate with bus voltage 4-40V. The waveform showing that the input voltage goes down to 0V and the spike goes beyond 60V. The high spike will damage the device. If you are trying to test out the device, probably use a smoother DC signal.
I'm wondering why there isn't a cap to smooth out the input signal?
Regards,
Yichi
Hello Haim,
If you disconnect our device and just probe the output of your bridge diode, do you still see the spikes? The fact that the input goes down to 0, and spike up to over 60V (please double check if it's from the output of diode rectifier or it's from our device) will cause our device malfunction. What I've seen normally is that people will add a cap at the output of the rectifier so that the output waveform is more stable DC. This will definitely help with the spike and UVLO issue.
Regards,
Yichi