Hi,
I have a problem by using the TS2 pin to wakeup the BQ from shutdown mode. The current necessary to detect a ground for the BQ in nearly 1µA. This could not be a problem but I need to use 3 switches in parallel to wakeup my board.
So I decided to make an OR function by using diodes. The problem is when the board is heating (nearly 40°C), the performances of the components fall down and the diodes are not correctly blocked. Others components like MOS transistors are place behind the diodes and have the same problem.
Another constrain is I need to detect the switches state on a µC supplied by one of the BQ internal LDO set to 3V3. So I do not have any other power source than the battery voltage and the BQ wakeup voltage.
So my questions are :
Do you have any example of multiple parallel ground detection for the TS2 pin ?
Do you know a way to know the state of the TS2 pin when it is used as a wakeup ?
Thank you,
Victor TEXIER