Other Parts Discussed in Thread: TL431
Hi,
I have been trying to develop a constant current flyback converter using UCC28740 IC. The required specifications are 80V 0.6A at full load, 40V 0.6A at half load, likewise the voltage output should adjust according to load, in all the cases the current must be constant at 0.6A.
For designing the component values I used the excel file attached below. I developed a prototype board for the same. The output of the prototype board was 40V to 42V and 0.66A. The reference voltage at TL431 was not 2.5V though the design was for getting 2.5V. Can I get suggestions where I have gone wrong?
Later on I came to know that the optocoupler feedback circuit is not required for my application as I don't need constant voltage. So how can I modify the circuit?