This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS54824: tps54824 application question

Part Number: TPS54824

Hi team,

could you help to confirm below question?

Please help to confirm whether the PG pin of TPS54824 can be pulled up to 1.8V, using 1.8VCMOS level standard?
In the following manual, only the maximum 6.5V limit is found, but it does not seem to mention how much voltage can be pulled up