Hi Team,
Can you please suggest best alternatives we can offer today to AP2202K-3.3TRG1?
Thanks in advance
Best Regards
Furkan Sefiloglu
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Furkan,
TPS7A2433DBVR would be the latest LDO that is p2p. There are also some older devices as per the comparison table below.
AP2202 | TPS7A24 | LP2985 | LP2985-N | |
AEC Q100 | NO | NO | NO | NO |
Output Options | Adjustable Output, Fixed Output | Adjustable Output, Fixed Output | Fixed Output | Fixed Output |
Iout (Max) (A) | 0.15 | 0.2 | 0.15 | 0.15 |
Vin (Max) (V) | 13.2 | 18 | 16 | 16 |
Vin (Min) (V) | 2.5 | 2.4 | 2.2 | 2.2 |
Vout (Max) (V) | 12 | 17.75 | 10 | 6.1 |
Vout (Min) (V) | 2.5 | 1.24 | 1.8 | 1.8 |
Fixed Output Options (V) | 2.5, 2.6, 2.8, 3, 3.3 | 1.25, 1.8, 2.5, 3, 3.3, 3.6, 5 | 1.8, 2.5, 2.8, 2.9, 3, 3.3, 5, 10 | 2.5, 2.6, 2.7, 2.8, 2.9, 3, 3.1, 3.2, 3.3, 3.5, 3.6, 3.8, 4, 4.5, 5, 6.1 |
Enable | YES | YES | YES | YES |
Power Good | NO | NO | NO | NO |
Output Capacitor Type | Non-Ceramic | Ceramic | Ceramic | Ceramic |
PSRR @ 100KHz (dB) | 30 | 22 | 40 | 30 |
Noise (uVrms) | 82 | 300 | 30 | 30 |
Accuracy (%) | 2 | 2 | 5 | 2 |
Vdo (Typ) (mV) | 165 | 160 | 280 | 280 |
Iq (Typ) (mA) | 0.095 | 0.002 | 0.065 | 0.065 |
Thermal Resistance θJA (°C/W) | 165 | 167.8 | 206 | 169 |
Min Package Area (mm2) | 4.64 | 4.64 | 4.64 | 4.64 |
Package Type | SOT-23, SOT-89 | SOT-23 | SOT-23 |
SOT-23 |
Regards,
Prakash L