Other Parts Discussed in Thread: BQ79616,
Hello TI team,
Myself Rakesh developing a Complex Device Driver (CDD) for BQ79616 ASIC for an Battery Management System project.
I am facing few issues listed below while testing with BQ79616 devices, request you to look into it and provide me a quick feedback.
- Accuracy of cell voltage measurement:
We observed that only VC0 pin is measuring accurate battery voltage where as other pins(VCx) are reading/measuring reduced battery voltage, difference is close to 1 volt.
- Comm diag errors:
BQ79616 devices are continuously reporting SOF and Daisy chain crc error even with single read operation@10ms,
- Fluctuation of VC pin measured voltages when CBFet open circuit diagnosis is performed.
VC pin measured voltages are fluctuating(10%) whenever CBfet open circuit diagnosis are performed.
- When cell balancing is active and if CB open circuit diagnosis is performed then it was observed devices are not responding. Do we need to pause cell balancing even for CBfet open circuit diagnosis?
I request you to provide a demo/sample code wherever possible which will accelerate/help our development activities.
Also guide us if we missed any preconditions or configurations.