Part Number: BQ25616
Other Parts Discussed in Thread: BQ24161B,
I have used BQ24161B in several designs. It works well, but there is one issue related to the CD_b pin (Chip Disable). This pin does more than just shutdown charging, it actually shuts down the chip as well. If the battery is very low and there is a charging source attached to VBUS, when the CD_b goes high, the system voltage drops as well, which causes the rest of the system to go down.
Now looking at the BQ25616, spec, it seems that the CE_b (Charge Enable) only affects charging. If there is a charging source present and the CE_b is driven high to shut off charging, does this only close the battery FET, while allowing the switcher to continue to provide a constant system voltage?
Matt