(1) Can the TPS24772 eFuse be used to protect an output? My system powers four external probes over a long cable. I need to protect the system power outputs against wiring faults to make sure that one wiring fault doesn't hurt the system or interfere with the other probes.
(2) Is there a way to force a retry after a Fast Latch Off event? Page 13 of the datasheet shows that there is no retry.
Could a retry be forced by shorting ENHIS to GND, or by shorting one of the timer pins to GND?
(3) Can theTPS24772 be used as a load switch by pulling ENHIS to GND?
Thanks!