This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25883: BQ25883 ADC_DONE INT rising edge is detected in what REG?

Part Number: BQ25883

The interrupt generated from the ADC_DONE_STAT is flagged in what i2c register? I see it can be masked as enabled/disabled in Charger Mask 1 (0x12) bit 7. But when an INT occurs when done, it *appears* to show up as bit 7 in REG0F (Charger Flag 1), but the data sheet indicates this as reserved bit.