Hi team,
we are using TPS22965 in our design and we want Vout rise time more then 50msec(miliseconds). the configuarations are
Vin = 5V
Vbias = 5V
Cin = 22uF
CL = 2.2uF
from the datasheet sec 9.3.1, Table 1 , CT value is given only upto 17700usec(17.7msec) . my queries are:
1. using the formula SR= 0.38*CT+34, can i use CT value of 0.047uF (47000pF), so i get a rise time more than 50msecs.
2. what is the maximum CT value i can use on this device.
--
Thanks in Advance,
Kiran