Hello,
What is the recommended shunt value for an application that can handle up to 50A from an 8S LiFePO4 battery pack? To keep the voltage below the 200mV limit I can use 4mOhms but the resistor would have to handle 10W. If I use two 8mOhm in parallel they would only have to handle 5W each.
In the BQ76942 datasheet section 18 (page 75) under Layout Guidelines the following statement has me concerned: " The device is designed to support a 1-mΩ sense resistor." Is it reasonable to use a 4mOhm sense resistor?
Thanks,
Richard