Hello,
I am interested in your LM3410XBSTOVPEV/NOPB demo board. In its User’s Guide (AN-1996), Figure 8, it states “The evaluation board can be modified to allow the user to derive the power from an input supply that is larger than 5.5 V.” How do you modify the evaluation board to perform the Figure 8 function?
If it can be modified, I would like to run off vehicle power (13.8V). I then can add a zener diode and resistor like your LM3410 data sheet shows (Page 28, Figure 28). For the final design, I would need 1A ran through 4 LEDs from the vehicles 13.8V supply using a LM3410XQMF/NOPB.
Thank you,
-Barry