Other Parts Discussed in Thread: TPS92612, LM3410
Hi Team.
My customer now use TPS92612-Q1 in charging the NiMH battery.
the input is 8V, the output current need to be 50mA.
Here are two questions about TPS92612:
1/ Whether it will become very hot when no load connect in the output? What will happen if no load in the output side?
2/ Does the output voltage is equal to 8V-dropout ≈7.5V?