Hi team
Could you help recommend the correct device for the following two requirements?
Boost #1
- Vin=5V/12V
- Vout=18V(Typ.) 20.4V(Max)
- Iout=500mA
It seems MC33063A is a good choice for this application?
Boost #2
- Vin=12V
- Vout=110V
- Iout=500mA
It seems LM5156 is a good choice for this application?
Thank you.