This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS7A24: C_OUT value

Genius 17295 points
Part Number: TPS7A24

Hello

TPS7A24 datasheet defines C_OUT value as 1 ~ 100uF with note "(1) All capacitor values are assumed to derate to 50% of the nominal capacitor value".

Does that mean C_IN must be 1uF+-50% ~ 100+- 50% = 0.5uF ~ 150uF including all errors?

Regards,
Oba