This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ34Z100-G1: MAX ERROR Rises from 1% to 116% and SOC falls from 44% to 33% after 3 days of relax

Part Number: BQ34Z100-G1
Other Parts Discussed in Thread: BQSTUDIO

Hello,

after doing multiple discharges and loads for 85 hours, the SOC ended up at 44% (which was fine).

but then, this happened: 
After 3 days of resting, the SOC value has decreased to 33% with max error of -116%. This is a problem we can't solve, could you helpe us?

You will find attached a screen sensor of the result, an export file of the datas and the cycles we ran with the battery 3 days before ir happened

Best regards,

YUNFENG

1507pb_apres_multiples_charges_decharge.gg.csvmultiples charges decharges.log