Other Parts Discussed in Thread: BQSTUDIO
Hi
We have designed a BQ40Z50-r1 4S1P Battery Pack.
i have two queries which is as follows
1.We have Uploaded a ,gg file and updated the battery chemistry , then we have charge at 1A,the battery is charging but when we give more than 1.5 A the battery charging gets terminates automatically and XCHG bits get enabled and cuts the charging of battery. The Battery protection parameters are not enabled at the time of charging at 1.5A.
2.Likewise i have done learning cycle on one battery pack and i have exported the .srec file The Same .SREC file can be used to program other packs without doing a learning cycle on those packs.
Expecting the reply at the earliest.
Regards
ANANDAN