This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24075: Vin / Vout question

Part Number: BQ24075

Hi Team,

My customer is surveying our BQ24075, they have one question here:

When the input voltage is lower than 5.5V + VDO (IN-OUT), is the Vout of BQ24075 will lower than 5.5V ?
Is there a charger IC with a fixed output greater than 5V and need to charge 4.2V/500mAh battery, please help to provide your recommendation.

Thank you!!

Kai