I'm seeing worst than expected transient response with PTH08T220W and type B bulk capacitors. After reviewing the spec, I'm wondering if I have the optimum turbotrans resistor value. I have a 470uF cap with 20% tolerance. What is the optimal turbotrans resistor value? Is it appropriate to use 470uF in the formula, or should it be 80% of 470?