Hi team.
When the bulk capacitor is small, there are line frequency(60Hz) ripple in output, which is caused by limited duty cycle. I think it should be 120Hz. Is there any wrong?
Br,
Nison
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi team.
When the bulk capacitor is small, there are line frequency(60Hz) ripple in output, which is caused by limited duty cycle. I think it should be 120Hz. Is there any wrong?
Br,
Nison
Hi Nison,
Based on your description, I agree with you this output voltage drop might caused by maximum duty cycle limitation. since UCC28742 has a CC mode function when the max. duty reaches to ~0.475 at low bulk voltage , It will start entry CC mode . then output voltage will drop. if the bulk capacitance can't be increased , you can try to decrease turns ratio of transformer Nps.
Thanks.
It's a little odd in your waveform is looks like the voltage drop are the same with different load condition 0.3A and 1A. can you share the design specification : input voltage range , output voltage , rated output current , transformer turns ratio , Lm , Bulk capacitance . and the test condition when you capture the waveform . if you can share the schematic , it will be more better.
Thanks.