Hi team,
My customer is evaluating TPS73250, he noticed that fig.10 current limit vs. vout was tested with TPS73233, can we provide a similar figure for TPS73250?
Or should we consider that the same as TPS73233, -0.2V~0.5V will be the short circuit range so current limit threshold will be decreased, and in 0.5V~5.0V range it will be typ. 425mA?
Also, the current limit has a min value of 250mA. in which condition will the min value occur? The application will have about 250mA current spike, so the customer is worrying if this will hit the current limit and bring problem.
Best regards,
Zeming