This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS54331: Output is abnormal

Part Number: TPS54331


Dear Expert

TPS54331DR is used in the motor drive DC-DC DC output voltage ripple or sawtooth wave power failure, the whole machine does not work or work abnormal.

Input 24V ,output 3.3V .

Output waveform.