Other Parts Discussed in Thread: TPS92200
Hi,
1) Can you confirm the analogue dimming resolution of the TPS54200. The datasheet suggests a PWM signal between 1% and 100% but what resolution can I dim to between these values in analogue mode? Will the TPS54200 resolve the difference in PWM duty cycle of fractions of a percent - e.g. 10.01% and 10.02%?
2) What are the buck regulator duty cycle limitations? Can this comfortably output 10.5V from a Vin=11.5V?
Many thanks