Part Number: LM25085
Other Parts Discussed in Thread: TPS62135
Hello,
I have included my schematic and layout below.
Vin= 12V-16.8V (4S lithium battery)
Vout= 12V
Full load= 3A
Fsw= ~1MHz
When running a stress test (Full load 3A for a full battery discharge from Vin=16.8V down to Vin=12V), I think the components are getting too hot (probably due to high Fsw). We should be able to solve that issue (reduce Fsw), but I am concerned about how the circuit is acting when hitting this thermal limit. Ideally it would turn off/on with some thermal hysteresis as stated in the datasheet: 170C/150C.
What I see is the output getting stuck in some low output voltage state while still sourcing current. Some details:
- I recreated the issue with Vin=16.5V and eLoad=3A. It only takes several minutes for the issue to occur. The output voltage falls to ~100mV, eLoad can only sink ~2A (so it's essentially shorting the output trying to get 3A), and input power supply is still at 16.5V sourcing only ~225mA. Thermal camera shows components reaching ~160C.
- To stop "shorting" the output I reduce the eLoad to 250mA. Output voltage rises to ~700mV and can supply all 250mA of load current. Input voltage still 16.5V and ~200mA. Components still around ~160C. (Fig1,2,3)
- I disconnect the eLoad completely. Power supply still at 16.5V and ~200mA (where is this current going?). Components still around ~160C. (Fig4)
- Power cycling the converter restores normal operation.
Some scope captures to expand on these details:
Fig1
Ch2 (purple): PGATE
Ch3 (blue): VOUT
Ch4 (green): VIN
Iin= 200mA
Iout= 250mA

Fig2
Ch2 (purple): SW Node
Ch3 (blue): VOUT
Ch4 (green): VIN
Iin= 200mA
Iout= 250mA

Fig3
Ch2 (purple): SW Node (emphasis on negative voltage during diode conduction)
Ch3 (blue): VOUT
Ch4 (green): VIN
Iin= 200mA
Iout= 250mA

Fig4
Ch2 (purple): SW Node
Ch3 (blue): VOUT
Ch4 (green): VIN
Iin= 200mA
Iout= 0.0A (eLoad disconnected)
L=2.2uH

PFET: DMP2040-UFDF-7
Diode: PMEG3020EGWJ
Inductor: NRS5024T2R2NMGJ
C26 VCC cap has it's polarity reversed in the schematic, but it is ceramic.
Any ideas what is happening?? Thank you very much! I can provide/collect any other info you might need.