This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5118: 14V/10A schematics review

Part Number: LM5118

Hi Sir,

My customer is developing a board to refer the 4 switch design of LM5118 for 4.2~60V-in to 14V-out with 10A output current.

Could you please help to check and advise the schematic?

Thanks for your support.

Input voltage: CAR_PWR (4.2V ~ 60V)
Output voltage/current: SYS14V (14V/10A)

SYS14V_10A_V01_20210716.pdf