Customer verify the Thermal parameter and need the data of "power dissipation & θJC" for LP2985.
Datasheet have no data could reference.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Andy,
For LP2985, the θJC=76.1.
See more information below.
θja | 208.2 |
θjc | 76.1 |
θjb | 52.5 |
Ψjt | 4 |
Ψjb | 51.8 |
Hi Kyle,
Thanks, one more thing want to clarify that DS has θja and it's showing 206, which one is correct?
Regards,
Allan
Hey Allan,
Sometimes there can be small changes like this as the team's tools continue to improve resulting. 208.2C/W is our most up to date value, however such a small change wouldn't be very noticeable in an end application due to part to part variation of their system (PCB fabrication, PCB assembly, IC variation, etc....).