HI All
The SLVAF11 document explains very well that the LC stable relationship
But I have a Phase Margin of TPS568230 is used as the example in the file Confuse
PM:(wcross)=180+PhaseDP(wcross)+PhaseRI(wcross) +PhaseESR(wcross)+PhaseDelay(wcross)
PhaseDP(wcross)=-tan-1(2a*W0*Wrocss/W0^2 *Wcross^2)
PhaseRI(wcross)=arctan(Wcross/WRI)
PhaseESR(wcross)=arctan(Wcross/WESR)
PhaseDelay(wcross)=-(TON*Wcross/2)*(180/3.14159)
In the example,
L=0.86uH at 8A loading
VIN=12V
VOUT=1.5V
FSW=600K HZ
Co=110uF ESR = total ESR is 0.6mohm
TPS568230 =270krad/s (43kHz)
ACP=29.3
Vref=0.6V
W0=√1/L*CO
W0=102814
Wesr=1/co*esr
Wesr=15151515
Wcross=(Acp*Vref*W0^2)/*WRI
Wcross=(29.3*0.6*102814^2)/270K=688271
PhaseRI(wcross)=arctan(688271/270K)=68.58
PhaseRI(wcross)=arctan(688271/15151515)=2.6
PhaseDelay(wcross)=-(0.2083u*688271/2)*(180/3.14159)=-4.107
TON =1/600KHZ *1.5V/12V=0.2083us
Since the range of PhaseDP (wcross) is -90 degrees to 90 degrees
PM:(wcross)=180+(-90~90)+ 68.58+2.6+(-4.107)
Since the range of PhaseDP (wcross) is -90 degrees to 90 degrees
It is impossible to approach it no matter what, the data is estimated to be 57.7 degrees