Hi,
I have a question about the configuration of UCD9240.
After I configured UCD9240, the data was stored inside UCD9240 and I don't need to configure it again for next power up.
Is my understanding right?
Thanks,
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
I have a question about the configuration of UCD9240.
After I configured UCD9240, the data was stored inside UCD9240 and I don't need to configure it again for next power up.
Is my understanding right?
Thanks,
Tony,
You are correct. The UCD92xx devices follow the PMBus standard. It states that the device is configured by writing to volatile registers/memory, then when you are satisfied with the configured operation of the controller, you store all these settings to non-volatile memory and they are applied on the next power-up. The PMBus command to do this is called STORE_DEFAULT_ALL.
When using the Fusion Digital Power Designer program, you write to the volatile registers by clicking the "Write to Hardware" button. To permanently store the settings to non-volatile memory, cliick the "Store RAM to FLASH" button.