This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Boost Converter IC with Current limiting feature

Other Parts Discussed in Thread: LM5155, TPS61390, TPS61391

Hi,
I need an IC which can boost single cell LiPo battery voltages to 50V and also have a current-limiting feature. I don't want current more than 0 to 30mA at the output either fixed or variable.
If a 50V boost converter along with the current limiting feature isn't available then I can use two ICs or some circuits to achieve it. 

Thanks